Extinction is described generally as a polarizing filter's ability to absorb polarized light that has an orientation 90° to the polarizer's axis of polarization.
The Extinction Ratio is the ratio of power for plane-polarized light going through a polarizer with its axis oriented parallel to the plane of polarization over the power of plane-polarized light going through that same polarizer with its axis oriented perpendicular to the plane of polarization (for example, 700:1). A more technical definition of Extinction Ratio, follows from the Handbook of Optics (Vol. I, 5-13):
Extinction Ratio = r = T2/ T1 » ½ (T^ / T|| )
where:
T1 = maximum transmittance parallel to plane of polarized beam
T2 = minimum transmittance perpendicular to plane of polarized beam
T|| = maximum transmittance of two polarizers parallel in unpolarized beam
T^ = minimum transmittance of two polarizers perpendicular in unpolarized beam
Note: all "T"; values are for monochromatic light.
Example: If using an unpolarized light source, a direct reading of the extinction ratio is not possible but can be estimated. If the unpolarized source has a wavelength of 550nm and the parallel transmission is 27.17% and the crossed transmission is 0.02%, then the extinction ratio at 550nm is approximately 3.7 x 10-4.
Polarization Efficiency is the percentage of how efficiently one polarizer polarizes incident light over the total amount of polarized light. For example, a linear polarizer with 99% efficiency transmits 99% of the incident light in the intended polarization (p-polarization state) and 1% in the opposite polarization (s-polarization state). Again a more technical definition exists, as based from the Handbook of Optics (Vol. I, 5-13):
Polarization Efficiency = P.E. (%) = [(H0-H90) / (H0+H90)]1/2 x 100
where:
H0 = average transmittance (unpolarized incident light) of parallel polarizers, over
400-700nm
H90 = average transmittance (unpolarized incident light) of crossed polarizers,
over 400-700nm
Note: "H" values are averages from 400 to 700nm (not the same as "T" values)
Example: If the source is again unpolarized and the average parallel transmission across the visible is 26.53% and the average crossed transmission across the visible is 0.01%, then the polarization efficiency is 99.96%
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics India Private Limited, #267, Greystone Building, Second Floor, 6th Cross Rd, Binnamangala, Stage 1, Indiranagar, Bengaluru, Karnataka, India 560038
California Consumer Privacy Acts (CCPA): Do Not Sell or Share My Personal Information
California Transparency in Supply Chains Act
The FUTURE Depends On Optics®